LTE FDD
Resets your current LTE FDD application configuration to default settings.
SCPI Command |
[:SOURce]:RADio:LTEFdd:PRESet |
SCPI Example |
:RAD:LTEF:PRES |
State Saved |
No |
Initial S/W Revision |
A.14.00 |
Opens a file management window where you can open a previously saved LTE FDD configuration file (*.pwsg).
When the LTE FDD setting file (*.pwsg) is loaded, the current waveform playback state is not changed.
For Real-Time Uplink capability, the state is kept after loading the settings, but need to toggle State OFF/ON to apply new settings.
SCPI Command |
[:SOURce]:RADio:LTEFdd:MEMory:STATe:RECall <string> |
SCPI Example |
:RAD:LTEF:MEM:STAT:REC "TEST1.pwsg" |
Notes |
Set only (Action) |
State Saved |
No |
Initial S/W Revision |
A.14.00 |
Ready for Test |
Y |
Opens a file management window where you can save your current LTE FDD configuration as a file (*.pwsg) for future use.
SCPI Command |
[:SOURce]:RADio:LTEFdd:MEMory:STATe:SAVE <string> |
SCPI Example |
:RAD:LTEF:MEM:STAT:SAVE "TEST1.pwsg" |
Notes |
Set only (Action) |
State Saved |
No |
Initial S/W Revision |
A.14.00 |
Opens a file management window where you can save your generated waveform file (*.wfm) for future use.
When a real-time carrier is selected, the Export Waveform feature is not available, and the menu is hidden.
SCPI Command |
[:SOURce]:RADio:LTEFdd:WAVeform:EXPort <string> |
SCPI Example |
:RAD:LTEF:WAV:EXP "WAV01.wfm" |
Notes |
Set only (Action) |
State Saved |
No |
Initial S/W Revision |
A.14.00 |
Opens a file management window where you can open a previously saved setup file (*.scp) to the waveform configuration.
Refer to the section of "Restrictions of PWSG version" under "Customer-Facing Feature Description" for difference between Signal Studio and PWSG versions.
When a real-time carrier is selected, the Import Signal Setup feature is not available, and the menu is hidden.
Importing of the *.scp file of Signal Studio LTE FDD Real-Time is not supported.
SCPI Command |
[:SOURce]:RADio:LTEFdd:WAVeform:FILE:IMPort <string> |
SCPI Example |
:RAD:LTEF:WAV:FILE:IMP "TEST01.scp" |
Notes |
Set only (Action) |
State Saved |
No |
Preset |
|
Initial S/W Revision |
A.14.00 |
Opens a file management window where you can save the current waveform configuration as a setup file (*.scp) for future use.
When a real-time carrier is selected, the Export Signal Setup feature is not available, and the menu is hidden.
Exporting of the *.scp file of Signal Studio LTE FDD Real-Time is not supported.
SCPI Command |
[:SOURce]:RADio:LTEFdd:WAVeform:FILE:EXPort <string> |
SCPI Example |
:RAD:LTEF:WAV:FILE:EXP "TEST01.scp" |
Notes |
Set only (Action) |
State Saved |
No |
Initial S/W Revision |
A.14.00 |